Part Number: DLPLIGHTCRAFTER
Tool/software: Linux
Dear Engineers:
I have a problem about how to use the API_DefinePatternPix on the DLP Lightcrafter (DM365) Platform. The function is declared in the file LCR_API.h.
The function prototype is listed bellow:
ErrorCode_t API_DefinePatternPix(PatternCount_t PatternNum, uint32 X, uint32 Y,
uint8 *Data, uint32 Count);
Could you tell me the meanings of the parameters. And how to use the API_DefinePatternPix function. Can I use the function to generate more than 96 images/patterns?
Thank you for your time!
Dong Cai