Part Number: DLP3000
Hello,
In general IP address for LC units is 192.168.1.99. But one that I cannot connect has the following properties. DHCP is not enable and its IP address is duplicate. How can I reset this to default values so that it works. Thank you.
Ethernet adapter Local Area Connection 4: Connection-specific DNS Suffix . : Description . . . . . . . . . . . : USB Ethernet/RNDIS Gadget #2 Physical Address. . . . . . . . . : 0A-2F-56-0B-38-CE DHCP Enabled. . . . . . . . . . . : No Autoconfiguration Enabled . . . . : Yes Link-local IPv6 Address . . . . . : fe80::51b6:20dd:8598:5945%23(Preferred) Autoconfiguration IPv4 Address. . : 169.254.89.69(Preferred) Subnet Mask . . . . . . . . . . . : 255.255.0.0 IPv4 Address. . . . . . . . . . . : 192.168.1.99(Duplicate) Subnet Mask . . . . . . . . . . . : 255.255.255.0 Default Gateway . . . . . . . . . : DHCPv6 IAID . . . . . . . . . . . : 744419992 DHCPv6 Client DUID. . . . . . . . : 00-01-00-01-21-B6-9C-19-3C-97-0E-1A-20-16 DNS Servers . . . . . . . . . . . : fec0:0:0:ffff::1%1 fec0:0:0:ffff::2%1 fec0:0:0:ffff::3%1 NetBIOS over Tcpip. . . . . . . . : Enabled