Hi,
We are using the DLPLCR4500EVM board with the DMD (without the light engine) for a custom microscope setup. We are using a tunable laser and we are encountering problems with diffraction. Since the DMD acts as a blazed grating, the reflected beam direction is highly sensitive on wavelength. However, if the mirrors could be set to be in "parked" position, we could use the m=0 order which is independent of wavelength.
Is there a way to control a set of mirrors to be flat or parked position (so not only "on" or "off"?) I understand the GUI provided by TI does not allow it, but if there is a way communicating directly to the controller without going through the APIs, or modifying the board or buying a different DMD with this functionality, we would highly appreciate the help.
So far I've only found a similar question on this forum (http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/advanced_light_control/f/924/t/607695?tisearch=e2e-quicksearch&keymatch=flat%20position) , but in the answers it was not addressed if choosing another DMD could solve the issue.
Thank you in advance for your help,
Joan