Part Number: DLPLIGHTCRAFTER
Hello TI,
I have an old verison v1 of the DLP Lightcrafter 3000 EVM, unvortunatelly it is not working completely correct. I can connect the GUI test software and upload static images, it is possible to change the test patterns and I can also read the pattern sequence settings but I can not upload other settings nor can I upload image sequences. When clicking upload, the software gives an error "command FAILED". I already tried to update to firmware version 5.0 but then the board does even not boot, this is why recently version 3.31 is used.
Do I need to add a 0Ohm resitor at position R205 in order to get the full device capabilities? Or did I miss something esle?
Thank you in advance...