We want to illuminate Alu mirror array with expanded (to area of mirror area) 100 fs laser pulse beam at wavelength of 800nm with 2-3W averaged power, How long we can do that without any destruction (100ms we have to do at minimum) - how long we have to switch of the beam after that?
How we should test the change of the mirror by heat-up the mirrors? What are the 100femtosecond laser parameter we can use at maximum? Is it possible to get another mirror type and safety glass - working with expanded 100 fs laser beam - 800nm wavelength / 80MHz and 2-3W averaged power -> for example dielectric mirrors or silver mirrors?