Dear Sir/Madam,
Hi. By far the only way I used to upload the images for pattern sequence mode is upload from insertion into the firmware and flash it into lightcrafter 4500.
From TI doc, it's mostly mentioned about using flash to upload the images inside embedded 48bit RAM for pattern sequence mode. I noticed it's taken quite a long time, almost 200 - 300 ms. Probably due to the decompression steps.
Is it possible to upload to 48bit RAM using RGB interface which is 120 frames/s? That would be 8.3ms per 24bit images.
Am I possible to upload the image to second 24bit buffer, while triggering the projection of images from another 24bit buffer with pattern sequence mode?
Thanks.