Hi,
I would like to know the reflectance v.s. wavelength relation of the micromirror arrays of DLP 4500 and DLP 4500NIR.
Thanks.
Sincerely,
Allen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I would like to know the reflectance v.s. wavelength relation of the micromirror arrays of DLP 4500 and DLP 4500NIR.
Thanks.
Sincerely,
Allen
Allen,
It is possible to replace the DMD used in the Lightcrafter4500 with a NIR version. However, the optical components are not coated to really take advantage of it. We do something similar in our LC4500 and offer either the standard visible window version of the DLP4500 or the NIR version. It is the same connector on the DMD package - you just need to be careful on avoiding fingerprints and take precautions on ESD.
Hi Paul,
We are planning on using the DMD4500 NIR to shape laser beams (with 1064 nm wavelength), more specifically, we planned to generate a ring beam by making the DMDs form a doughnut pattern and shine laser onto it. I guess that we will eventually remove the LEDs and replace them with our laser beam. The mirrors and lens inside will be removed for convince, leaving only the DMD and the control board.
If my memory serves me correctly, my colleague in the lab and I have both read a official document on DLP4500 that says by replacing the DMD4500 on DLP4500EVM with DMD4500NIR, we can then shine 1064nm wavelength on it with better efficiency and gain control of the DMD4500NIR in the same way.
Can DLP® NIRscan Evaluation Module help us achieve our goal?
Thanks,
Allen
Hi Adam,
Can you give me a quick introduction on your company's product and how it works with TI's DMDs and DLPs? I am now really confused by all the versions and products on the internet. Besides, can you tell me how it works to swap the DMD4500 with DMD4500NIR on Libghtcrafter 4500?
Great Thanks,
Allen
Allen,
I'll give you the short answer, feel free to call us or contact us directly if you have further questions.
* For general pattern control, you can use the electronics from the LightCrafter 4500 module and replace the DMD with the DLP4500NIR. The limitation of the Libghtcrafter electronics is that their is a rather short flex-cable (1-2 ") between the DMD and the main control board, making it a bit of challenge to mount on any bench optics.
* We specifically designed our own LC4500 controller board, that is compatible with the TI API and GUI, that has a cable interface to the DMD holder board. It comes with either the standard or NIR DMD. It also has a optional expansion board that allows you to quickly download an BMP file for patterns (instead of flashing a new image file).
* The NIRscan is specifically designed for spectroscopy. While it uses the DLP4500NIR, the electronics don't seem well suited for your project.
I hope that helps clarify things. It can be a bit confusion between all of the solutions that TI offers and what the various Design Network partners offer.
Allens,
Sorry for my delayed replay. Best way is to submit a contact form at http://www.keynotephotonics.com/contact-us/ and someone will follow-up with you further by e-mail or phone.
Hi Yong,
Yes, we can configure a kit that includes the drive board, the DLP4500NIRFQE, and cable. The same TI API will work directly with this kit to communicate to the DLPC350. We provide an updated GUI tool that supports the particular flash memory installed, as well as control some other functions. It looks and operates very like the TI version.
Dear Yong,
These are good questions.
1) The DLP4500NIRFQE less expensive due to the package design. I'm not sure your application, but unless you plan to create high-power IR design, I would recommend using this. Also, the mechanical interface to use the FQD package is more difficult and may require some custom mechanical design to ensure the DMD is attached to your optical system.
2) The software is available at no extra charge. We can provide a quote for the drive board and DMD. Please go to our contact form at keynotephotonics.com/contact-us and we can send it to you directly. We can also send you user's guide.
You can also find the entire kit on our e-store at LC4500-NIR-EKT
Oh I understand, so you mean I can get DMD from the agent of TI but I can't get the drive board from TI, but how can I get the drive board from the agent because I am in China? Thank you. Expect your reply.