Tool/software: Lightcrafter 4500
Hi,
when i use the LightCrafter 4500 Graphical User Interface control software, and the softeware is 3.0.1 version. I want to set the operating mode in "Pattern Sequence"mode, when I set the BIT PLANE SELECTION, and add the pattern to sequence,I clicked the "G0,G1,G2..." and the add pattern to sequence, but I can't clicked "B5,B6,B7'' on the GUI,and I can't find them.Just like the photo below where I marked in red pen.I tried other version of the GUI and there are also the same problems. Maybe there are some problems in the software compilation and need to recompile but I didn't configure the QT Library and I don't know how to rebuild it .So could you sent me another SDK which will be rebuilt? Thank you very much!