Other Parts Discussed in Thread: TIDA-00254, DLPLCR4500EVM
I have used DLP 4500 EVM for 2 months. I can realize line pattern scanning by using the pattern sequence. The camera I have used is Point GrayBFLY-PGE-50A2M-CS and the capture mode is free running. but now here came the problem. If the pattern period is too short, the pictures captured by the camera will miss.
So I want to realize the synchronization between DLP 4500 and Camera.
I have read your example application on 3D vision. And I have prepared the cable to connect the DLP and Camera.
But I am still confused about how to configure the trigger signal through the GUI if i want to make DLP to trigger Camera? I saw the trigger control parameter in the pattern sequence mode.
if i need to make my line pattern period and exposure is 100ms, how do I configure the trigger signal to make the camera capture each pattern?
I am looking forward to your reply
Thank you very much.