Support Path: /Tools & software/Help find tools and software/Design Kits / Evaluation Modules / Boards/
Hello,
My name is Larry Sanders and I'm working with the University of Dayton. I have a project doing something similar to edge detection where I'm display the negative image using the 4500 EVM. I want to use the bit streaming method (I believe it achieves 120 Hz) to display the negative, binary image. I have the GUI source code, but I'm having trouble parcing through it to get the info I need. Could someone point out the following for me:
-What general setup needs to be performed?
-How do I enable the bitmap streaming?
-How do I load a new bitmap to be streamed?
Again, if someone could point these out in the source code or provide examples I would greatly appreciate it.
Thank you,
-Larry Sanders