Hi,
Let me talk about flip of DLP4500.
My customer want to use flip of West/East on Pattern Sequence mode.
But Diagonal line in Image is broken after flip like this.
Because of Diamond array.
Is there a way to avoid this ?
Best Regards
Hiroyasu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Let me talk about flip of DLP4500.
My customer want to use flip of West/East on Pattern Sequence mode.
But Diagonal line in Image is broken after flip like this.
Because of Diamond array.
Is there a way to avoid this ?
Best Regards
Hiroyasu
Hi, Kyle
Thank you for your reply.
My customer use Pattern Seqence mode and store Data in Flash.
Actually We see this issue on DLP4500 EVM.
and They can not increase bit plane.
Because My customer need 90 bit plane for continuously output.
I understand it can store upto 48 bit plane in internal memory
They will make 90 bit plane using flip.
We need to improve or avoid to this issue.
Best Regards
Hiroyasu
Hello Hiroyasu,
Could you go into a little more detail about how you produced this issue? It would be helpful if you could send me an example pattern where you see the issue. Also how are you evaluating the issue exists? Are you taking a picture to spot the issue. After I get these details hopefully I can better address the problem.
Thanks,
Kyle
Hi, Kyle
O.K. We evaluate East/West of flip using DLP4500 EVM and GUI.
After Binary Download using GUI, I click East/West button on GUI,
In this case, This image is broken after flip like I upload image.
I have binary file and image file for this evaluation.
but I can not send you this. Because this is customer's binary.
Can you send me mail this address ? If you like
If you give me mail, I can send you Binary and image file.
Best Regards Hiroyasu