Other Parts Discussed in Thread: DLPC350
Hi,
I'd like to use the LightCrafter 4500 EVM to stream 8bits pattern while being pixel accurate. As far as I understood the user guides and datasheets, it is impossible to bypass the image processing in Video mode so I'm trying to use the pattern sequence mode. Everything is working as expected the only issue is that the sequence is not automatically starting after powering up the EVM. Sending a "play" command through USB is necessary. I'd like to have the sequence starting automatically without sending a "start" command, but this seems to be a "known limitation" as explain in this thread regarding the same issue:"How to start sequence automatically after boot"
So my question is :
As I don't want to connect the EVM with USB, would it be possible to use GPIO on the board to send the starting command via I2C once the device is properly initialized ? With such a solution I would only have to connect some GPIO to the I2C connector.