Other Parts Discussed in Thread: DLPC350
Hi,
Let me talk about DLP4500.
When update the FW via the I2C from the application of the FPGA, there are cases where it fails as follows.
A) I2C communication fails (I2C bus busy) during image transfer with Download Data (I2C: 0x25).
B) Even if download data (I2C: 0x25) of DLPC 350 is executed with length "none"
After sending the image with Download Data (I2C: 0x25) for the size set by Download Data Size (I2C: 0x2C)
The checksum calculated by Calculate Checksum (I2C: 0x26) is different from the checksum calculated on the program.
As a tendency, the failure rate is high when the size to be transmitted with one Download Data (I2C: 0x25) is large.
In our environment, it succeeds if it is 15 bytes or less. But It failed in A or B in 26 to 254 byte.
Could you give me some advice ?
Best Regards
Hiroyasu