Hi,
I am speaking on behalf of my team of three MSc students Earth Sciences from the University of Amsterdam. We are participating in the Spin Your Thesis! campaign hosted by the European Space Agency. We will execute an experiment in a hypergravity simulator called the Large Diameter Centrifuge (LDC, link for more info below) in September 2018, with the aim of examining the influence of gravity on granular avalanches. We are simulating small-scale granular avalanches under varying gravity conditions and wish to use the DLP Lightcrafter 4500 to create a 3D profile of the avalanches. We were inspired by an article from Deetjen et al. (2017, the full reference can be found below), where they use the device to make high-speed surface reconstructions of a flying pigeon. To use in our own experiment, we have some questions regarding the application of the DLP Lightcrafter 4500 that we could not find in the user's guide.
-
What is the minimum distance from the Lightcrafter to the object the laser grid will be projected on (the avalanche in our case)? We have limited space in the LDC gondola, so the DLP Lightcrafter 4500 would be placed about 30 centimeters max. from the surface.
-
Is it necessary to have a specific camera with the DLP Lightcrafter 4500? We have read something about the Fire Wire, but are wondering whether there is also the possibility of using for instance a regular Nikon or GoPro camera or any other options.
-
Does the Lightcrafter have a minimum size of the studied object, or what kind of spatial resolution are we speaking of? Our avalanches will have height differences of less than 1 millimeter, which we would want to be visible in the laser grid.
Could you give us some advice?
Deetjen, M. E., Biewener, A. A., & Lentink, D. (2017). High-speed surface reconstruction of a flying bird using structured light. Journal of Experimental Biology, 220(11), 1956-1961.
More info on the LDC: https://www.esa.int/Education/Spin_Your_Thesis/The_Large_Diameter_Centrifuge2
Thanks in advance and kind regards,
Carlijn Snoek