• TI Thinks Resolved

Discovery 3000 PROM programing

Hi,

I`m currently developing new imaging device using a DLP Discovery 3000 board.  When trying to upload software into the prom (xcf08p), it stops after only 4% without any error message.  So I have to reload the software manually on the FPGA each time I turn on the board.  Does someone have any idea of what could be the cause of this problem?

Thanks,

  • Hello Samuel,

    It is great to hear you are devloping a new device based on the D3000.   It will be best to contact the VAR (value-added reseller) you purchased the kit from to address your specific question.   If for some reason that path doesn't solve your problem, let us know and we'll help get you an answer. 

  • In reply to GPark:

    Hello GPark,
    I have a DMD Discovery D3000 Development Kit,but i want to make another board connectting to it with port J3 and J4,and i have no information of the port dimensions on the D3000 board.Can you send me the Mechanical Dimensions of this Kit,including the Locating hole etc. thank you
  • In reply to user3929079:

    Hi user3929079,

    It will be best to contact the VAR (value-added reseller) you purchased the kit from to address your specific question. They can provide the accurate dimensions for the D3000 Development Kit that they sold.

    Regards,
    A214529