Hi,
I'm asking this question on behalf of another engineer. It is formulated like this:
In the datasheet to dlpc3500 note 16 on page 16 states: “The MOSC input cannot support spread spectrum clock spreading.” On the other hand, on page 53 one can read: “Note that the DLPC350 controller can only accept 0%, ±0.5%, and ±1.0% (center-spread modulation), and a triangular waveform.” Does the DLPC350 support spread spectrum or not?
Thanks in advance.
Kind regards,
Gustaf