Other Parts Discussed in Thread: TPS65145
HI
Now DLPC900 is working, dmd6500 is not working yet.
I can be sure that there is no problem with the electrical connection of the power supply ,so i measured the power of the DMD , VOFSET = 1.41V VRSET = 0V VBIAS = 0V VCC = 3.3V ,DMD mount whether or not the result is the same.
I experiment on EVM, do not mount DMD: VOFSET = 2.96V VRSET = 0V VBIAS = 0V VCC = 3.3V, mount DMD: VOFSET = 8.54V VRSET = -9.95V VBIAS = 15.91V VCC = 3.3V.
So what should I do next? Look forward to your advice.