I want to use a 532 nm laser light to illuminate the DLP7000, and expect that the reflected light is vertical to DLP7000's flat state. In this situation, DLP7000 can works in off state or on state. I am wondering if both
stated can be used, and whether they are same or not. Because when I let it work in off state, a strong diffraction is seen, which is not good for my system.
I will appreciate it very much if anyone can help me.
Thanks in advance.