This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] DLPD4X00KIT: Data input for DLP Discovery 4100

Part Number: DLPD4X00KIT

What type of input does the DLP Discovery 4100 use?

  • The DLP Discovery™ 4100 is Texas Instrument's most flexible and powerful DLP® technology platform. It allows users the lowest level control over the DMD, and as such, the data coming into the controller is simply binary data. The user interface for the application will have to be built to handle RGB or grayscale data such that it is fed to the device correctly. Please consult the datasheet and associated technical literature on the DLPC410 for further information.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.