Hi,
We designed DLP6500 projector based on the LightCrafter 6500 EVM. But recently, the flash memory M29DW128G70NF6E is out of stock.
So we must replace the flash M29DW128G70NF6E. As the file "FlashDeviceParameters" which TI suggested, I got the flash MT28EW128ABA1H and MT28EW256ABA1H. Now I used the flash MT28EW256ABA1H to replace the flash M29DW128G70NF6E. I found a strange problem, when I programed the DLPC900 firmware 2.0, the DLP6500 projector is working abnormally and the pattern mode can't display, but when I programmed the DLPC900 firmware 4.2, the DLP6500 projector works normally with the pattern mode. Another problem is existing, if I have programed the firmware 2.0 to the flash MT28EW256ABA1H, I can't program the firmware again and the GUI will be unresponsive or can't enter the program mode. So I want to know whether I can use the flash MT28EW128ABA1H or MT28EW256ABA1H to replace the flash M29DW128G70NF6E.
Another need to be noticed, the DLPC900 chips are purchased recently. I am not sure whether upgrade the DLPC900 chip so that we must program the firmware 4.0 or later.
Thanks for any help.
Best regards,
Kelly Yang