Dear TI community,
After powering-up and getting to the homepage, the Download Scan Data Files and the Slow Scan buttons are missing. I am using Win 7 and Chrome.
I made no other installation than the RNDIS driver
Thanks a lot for your insights!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI community,
After powering-up and getting to the homepage, the Download Scan Data Files and the Slow Scan buttons are missing. I am using Win 7 and Chrome.
I made no other installation than the RNDIS driver
Thanks a lot for your insights!
Hi Paul
Thanks, I installed DLPR350PROM-3.0.0. How shall I check for SW/FW versions?
Scans function but only in the 1350-2050 nm range
Regards
Hi Frederic,
I think the issue is that the NIRScan EVM is not compatible with the newest version of the DLPR350 FW, you need v2.0. Do you have a copy of that FW you can load onto your device?
Thanks,
Paul
Frederic,
Version 3.0 of the DLPC350 firmware should work with the NIRscan Application software v2.x. The NIRscan Application software requires v2.x or greater of the DLPC350 firmware.
Just to summarize,
Best regards,
Pedro
Dear Pedro,
Thanks for your answer.
Following Appendix C.1, I managed to create a SD card that was renamed 'BEAGLE BONE' and contains 2.19 Mb of files.
Then, I tried to follow Appendix C.3 but there is no reaction (GUI not displaing) )when plugging the device (point 4).
The C:\Texas Instruments-DLP folder contains the following:
DLPLCR4500GUI-2.0.0
DLPR350PROM-3.0.0
NIRscan_2.0.0
Kind regards,
Frederic
Hi Paul and thanks for your answer,
In the DLPLCR4500GUI-2.0.0 folder, LightCrafter4500 is the only available .exe (others are application extensions).
Still no reaction when plugging in, any idea?
Thanks for your quick feedback
Frederic