Other Parts Discussed in Thread: DLPC350, DLPC150
Hi, I'm using the DLPNIRSCANNANO (GUI v2.0.2, DLPR150PROM 2.0.0) from some months and it has worked well.
Now it has a problem, when I start the GUI an error message appear:
I click OK and then another error appear:
I click OK and the GUI is opened.
When i try to set the Scan Config from the GUI, the library is empty:
I think that there is a problem with the Scan Configuration saved on the device.
I tried to update the TIVA firmware and the DLPR150PROM but it dosen't work.
Could you suggest a solution to this problem? Is it possible to restore the Scan Config on the device?
Thanks in advance
Best regards
Nicola