I'm communicating with the NIRSCANNano device over Bluetooth. I'm able to download, deserialize and interpret a scan configuration just fine. However, what is not clear to me from the documentation is how I *upload* a scan configuration (after serializing it) to the device? Is this not supported?
When I look at the GATT Command Service (pg 99 in the manual), it seems that the maximum Command Data Packet size for Write (i.e. upload) is only 20 bytes where a serialized Scan Configuration payload is much more than that? (>90 bytes in my test case).