I think I have not understood how the following are related:
1) Optical Resolution = 10 nm
2) Digital Resolution = 228 (default factory config stored in the EVM)
3) Width in nm = starts from 2.34 in the config window
In the Scan configuration window, for default settings of Column1, I see the following :
"Saved in Nirscan Nano"
Wavelength range : 900 - 1700 nm
width in nm : 7.02
num of wavelength points : 228
Digital Resolution : 228
A) From the scan results that I have shared (for which I used the default factory Column 1 scan config), difference between 2 wavelengths is 3.89 nm.
B) for the factory default, 1700 - 900/228 = 3.50 nm. This does not match the "width in nm". Is it supposed to ?
How are these factory default settings and the scan results related to the optical resolution of 10 nm ?
Is "Digital Resolution" same as "Optical Resolution" ?
Why does A) not match "width in nm" or B) or "Optical Resolution" ?