Other Parts Discussed in Thread: DLP2010NIR, DLPC150
We would like to use the DLPNANOEVM to acquire 100 spectra per second in the range 1150- 1350nm with 12nm resolution. Looking at the GUI, the minimum exposure time is 0.635ms so it should be feasible.
When trying these settings we realize that the total scan time is much longer than expected (even keeping the lamp on and using a fixed PGA gain).
What is actually preventing us to achieve the desired scan rate? is that feasible with the current FW/GUI provided with the DLPNANOEVM or do we need to modify the FW/GUI?
Thanks a lot in advance.
Salvatore