Which is correct between datasheet and schematic?

Hi,

 

There are differences between datasheet "DLPC200.pdf DLPS014B" and Logic's Schematic. Which is correct?

 

Datasheet                          Schematic

PORT1_D10  port G3                 PORT1_D10    port G2

USB_CLK    port A15                USB_CLK      port B15

No description                     USB_RSVD_14  port A15

No description                     RSVD_X1      port AD15

No description                     RSVD_X12     port U8

No description                     RSVD_X13     port U7

No description                     RSVD_X14     port AB17

 

Best Regards,

 

keisuke