• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » DLP & MEMS » DLP LightCrafter Development Platform » Supplying external 1-bit monochrome patterns via HDMI
Share
DLP & MEMS
  • Forums
Options
  • Subscribe via RSS

Forums

Supplying external 1-bit monochrome patterns via HDMI

This question is answered
Gabriel Rosenhouse
Posted by Gabriel Rosenhouse
on May 09 2012 13:24 PM
Prodigy50 points

Hello,

I'd like to display external 1-bit monochrome patterns with the LightCrafter at the maximum frame rate (24 * 60 Hz = 1440 Hz) and supply the "patterns" via HDMI.  I don't care about the LEDs, since I will be using an external light source.

1) Is this possible? 

2) If yes, can I get that by setting sending the TCP/IP command for  "Video Mode Setting (0x02 0x01)"? 

3) On page 28 of the LightCrafter users's guide it says  "where this image enhancement is not desired, the video processing algorithms can be bypassed and replaced with a specific set of bit planes."  How do I do that?  I just want raw 1-bit images very fast, nothing else.

Thank you for your time!

-Gabriel

external pattern hdmi
Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Sanjeev
    Posted by Sanjeev
    on May 10 2012 01:08 AM
    Verified Answer
    Verified by Gabriel Rosenhouse
    Expert5535 points

    Hi Gabriel,

    Welcome to DLP & MEMS forum.

    Response to your questions.

    (1) Yes.

    (2) You need to call additional TCP/IP commands.

    Here's the sequence -

    Step-1)  Set Video Input Setting (02 00)  

    step -2) Set Video Mode Setting (02 01), Select 60Hz, Bite Depth = 1,  and then select Byte 2 = Monochrome Display

    Step-3) Change Current Display Mode (01 01) - HDMI Video Input

    (3) You don't need manual step of disabling the image processing algorithms. The Step(2) (as explained above) setting will take care. Basically in the step-2 when you mention Byte2 = Monochorme the DM365 automatically configures DLPC300 by sending algorithm processing disable commands.

    Regards,

    Sanjeev

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Gabriel Rosenhouse
    Posted by Gabriel Rosenhouse
    on May 10 2012 15:32 PM
    Prodigy50 points

    Thank you Sanjeev for the quick response.

    I'm currently troubleshooting the USB/RNDIS stuff (I've got it working sporadically on 1 computer, but not at all on another).  I will post an update once I've gotten to the point where I can reliably open a TCP/IP socket to the device.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Daniel Hochbaum
    Posted by Daniel Hochbaum
    on May 10 2012 15:36 PM
    Prodigy120 points

    Dear Sanjeev,

    Can this be done through the GUI? You can select a bit depth of 1 in HDMI input mode, but does it realize that this should be a monochrome display? When I look at the power spectrum of the HDMI display in 1 bit depth mode I see many high frequency peaks I'm associating with the image processing algorithms. When I use a 1 bit pattern sequence, the images displayed lack these high frequency peaks, so the image processing algorithms are disabled in this mode.

    Daniel

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Gabriel Rosenhouse
    Posted by Gabriel Rosenhouse
    on May 10 2012 15:41 PM
    Prodigy50 points

    Daniel, I'm curious how you're gathering this data, because I may want to do a similar diagnostic...Are you using a high speed camera to capture the projected image, or are you looking at some electrical signal on the board?

    Thanks...

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Daniel Hochbaum
    Posted by Daniel Hochbaum
    on May 10 2012 16:03 PM
    Prodigy120 points

    I'm using a high speed camera. My setup is as follows: I removed the light engine and am using an external laser source for illumination. I am imaging the DMD onto a fluorescence microscope sample plane. For diagnostics, I use a fluorescence bead sample, whose emission I am capturing on a CCD at ~1khz for 10000s of frames. I analyze the image by taking power spectra over illuminated areas in my movies. I've isolated the noise to the DMD, I saw similar power spectra when working with the pico projector. I could remove those high frequency peaks by talking to the pico through I2C and turning off all the spatio-temporal dithering.

    Daniel

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Sanjeev
    Posted by Sanjeev
    on May 11 2012 02:05 AM
    Expert5535 points

    Hi Daneil,

    Answers to your questions.

    Can this be done through the GUI? [Sanjeev] YES

    You can select a bit depth of 1 in HDMI input mode, but does it realize that this should be a monochrome display? [Sanjeev] If you select bit depth < 8 it always gets into mono-chrome display with image processing algos turned off. If bit depth = 8 AND RGB check-box unchecked then also DM365 will disable image processing algorithm. The default HMDI Video setting is 8 bit depth and RGB checkbox selected only this configuration the image processing algorithm in the DLPC300 will be kept active by DM365.

    When I look at the power spectrum of the HDMI display in 1 bit depth mode I see many high frequency peaks I'm associating with the image processing algorithms. When I use a 1 bit pattern sequence, the images displayed lack these high frequency peaks, so the image processing algorithms are disabled in this mode. [Sanjeev] Is this information sharing or do you have any question let me know.

    Regards,

    Sanjeev

     

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Gabriel Rosenhouse
    Posted by Gabriel Rosenhouse
    on May 13 2012 17:29 PM
    Prodigy50 points

    Thanks Daniel.  I was considering doing something similar with a linear photodiode array in order to sample (a line from) the image at a higher rate than the DMD updates, and verify that it was operating how I expect.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • hai jiao
    Posted by hai jiao
    on Jul 28 2012 03:59 AM
    Prodigy110 points

    Hi Sanjeev,

    I’m also trying displaying 1 bit depth monochrome images at 24*60 = 1440Hz, I have a video stream of 720*480@60Hz 24bit/pixel feeding into the mini HDMI port on the LightCrafter, I tried several settings but failed, can you tell me how to set the GUI to achieve that? And is there frame resolution limitation for this option?

    Thanks,

    Hai

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use