• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » DLP & MEMS » DLP LightCrafter Development Platform » LIghtCrafter Flexible Trigger Configurations
Share
DLP & MEMS
  • Forums
Options
  • Subscribe via RSS

LIghtCrafter Flexible Trigger Configurations

LIghtCrafter Flexible Trigger Configurations

  • PedroGelabert
    Posted by PedroGelabert
    on Jun 28 2012 11:43 AM
    Intellectual1990 points

    LightCrafter offers several flexible trigger configurations. The trigger connector (J7) lies at the back of the System board (top board):

    The pinout of J7 connector is:

    • Pin 1 - Tigger Supply
    • Pin 2 - Trigger Input
    • Pin 3 - Trigger Output
    • Pin 4 - Ground

    Two matching four pin mating connector part numbers are:

    • Molex part number: 51021-0400
    • Digi-Key part number: WM1722-ND

    The corresponding crimps part numbers are:

    • Molex part number: 50079-8000
    • Digi-Key part number: WM1142CT-ND

    LightCrafter's J7's trigger input and output pins are level translated or shifted to and from the I/O supply of circuits in the System board. Out of the factory, the output trigger signal is level shifted from the 1.8V I/O supply used by the System board FPGA to 3.3V. Below is a snapshot of the schematic of these circuits. U20 level shifts the trigger input. U23 level shifts the trigger output. Note that the supply on one side of these level shifters is tied to the internal 3.3V supply, while the other side is tied to 1.8V.  The level shifter are open-drain outputs with internal 10Kohm pull-ups.

    In this schematic, a resistor with a value of NA_0 indicates the resistor is not populated. A resistor value of 0 indicates that a zero ohm resistor is present.

    If an external 5V trigger signal is desired, then the LightCrafter board must be modified to input an external supply and use that as the level shifter input voltage, as follows:

    • Install zero ohm resistor R285
    • Remove zero ohm resistor R282

    Then supply the external trigger voltage through Pin 1 of J7 (EXT_TRIG_VCC) and the external trigger through Pin 2 of J7 (TRIG_IN_CON).

    trigger trigger lightcrafter input voltage synchronization
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Enio Alburez
    Posted by Enio Alburez
    on Apr 16 2012 18:19 PM
    Prodigy70 points

    Hi Pedro, I need some help interfacing a 5V MCU with the LghtCrafter Trigger inputs.

    I would like to know if there is a simpler way of doing it, without modifying the system board.

    I couldn´t find the R282 0ohm resistor. Where is it?

    Thanks

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • PedroGelabert
    Posted by PedroGelabert
    on Apr 19 2012 15:42 PM
    Intellectual1990 points

    Enio,

    Unless you have a level shifter on the MCU to change the 5V signals to 3.3V, you will have to modify the board. 

    R282 is in the back of the SyStem Board (top board). It is in the group of three resistors that has a label next to the daughter card connector. It is between the daughtercard connector and screw hole, next to a ground test point.  R282 is the middle resistor. 

    See the bottom left corner of this photo:

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Enio Alburez
    Posted by Enio Alburez
    on Jun 08 2012 12:34 PM
    Prodigy70 points

    Pedro, I have a few quiestions about the trigger signals:

    1. Which is the treshold voltage for 3.3V and for 5V?
    2. Can I power a circuit from the EXT_TRIG_VCC pin, how much current can I source
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • PedroGelabert
    Posted by PedroGelabert
    on Jun 08 2012 14:33 PM
    Intellectual1990 points

    Enio,

    The threshold voltage for TRIG_IN_CON is handled by the TXS0101. From its data sheet, the Vil is 0.15V and Vih is Vcc - 0.2V where Vcc is the EXT_TRIG_VCC. Vcc can be anywhere between 2.3V to 5.5V.

    You can power a circuit from EXT_TRIG_VCC. The amount of power is dependent on how much is consumed on the LightCrafter and the supply that is sourcing it. For instance, EXT_TRIG_VCC supports, 1.8V, 3.3V, and 5V options.

    • On default configuration of LightCrafter, the 5V supply is sourced from USB VBUS. So there is very little 5V current consumed in the system and the budget is dependent on what the USB port provides. On this supply, there is a TPS60150 (U25 in system board), but it is disabled and the P5P0V supply is disconnected from SYSPWR (the LightCrafter power input).
    • The 3.3V supply is sourced from the driver board TPS63020 (U15 in driver board) that has a max output current of 3A. However, this supply is used for most of the LightCrafter devices. So a significant budget is consumed, but it is not the majority of this supply. To provide an example when LightCrafter is operating at the 20 lumen value (LED set to 274), the overall current consumed at SYSPWR is about 700mA. This includes all the supplies including the LED drivers that use 600mA.
    • The 1.8V supply is sourced by the TPS650531 (U15 in system board) has a max rating of 1A.  This supply is shared with some DM365 analog and DDR2 I/Os, as well as, the DDR2 RAM so a few 100mA's are consumed when the DM365's external RAM is heavily used. 

    Note that the overall power budget is limited by the power supply into the LightCrafter system. This typically ranges between 2-3A. As you can see, there is enough current available on these supplies to power at least 100mA external circuit.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Enio Alburez
    Posted by Enio Alburez
    on Jun 11 2012 13:16 PM
    Prodigy70 points

    Thank you for the response Pedro.

    I have a few more questions:

    1. I'll be powering a circuit with 3.3 V, to do that I have to solder  0 ohm resistance R285 or R295 (please correct me if I'm wrong). Are these also located in the back of the System Board?
    2. Is there any conection to the 3.3V power source of the lightcrafter, that does not require a modification to the board.?
    3. Do you have the digikey part number for this 0 ohm resistors?
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Divya
    Posted by Divya
    on Jun 28 2012 11:43 AM
    Expert3690 points

    Hi Enio,

    You will have to install 0 ohm resistor at  R295,  which is on the top of system board (above the J7 connector).

    Here is the part number for 0 ohm resistor we used:

    Digi-Key part number: P0.0AGCT-ND , Manufacture part number: ERJ-1GE0R00C

    Could you please tell me how much current would the external circuit consume?

    Please be aware of the current you can source from this pin. (Refer to Pedro's post above).

    Regards,

    Divya

    www.ti.com/mems

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Jakob Wilm
    Posted by Jakob Wilm
    on Jan 17 2013 10:26 AM
    Prodigy65 points

    How would I be able to achieve a flexible output trigger configuration?

    Industrial cameras currently use triggers of different voltage (e.g. Point Grey Flea 3V and IDS Imaging uEye 5V).

    My idea would be to either move the zero-ohm resistor from R292 to R295, and source the appropriate trigger voltage from the camera itself, as most cameras provide some current at the right voltage.

    The alternative would be a three position microswitch installed over R291, R292 and R293. Does anyone have experience with this and can you recommend a part that could be soldered directly onto these positions?

    As most newer cameras use opto-isolated trigger ports, I wonder if one of these solutions offer an advantage in terms of current to drive the opto-isolated circuit? Also in the application note for "Imaging Source Cameras", it is suggested to output the trigger on pins 1 and 3, which reverses polarity. Does this mean more current?

    Regards,

    Jakob Wilm

    Technical University of Denmark

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Divya
    Posted by Divya
    on Jan 17 2013 16:52 PM
    Expert3690 points

    Hi Jacob,

    We have tested the scenario mentioned in white paper i.e, externally triggering the LightCrafter by installing 0 ohm resistors at R292 and R295. But if your camera is capable of sourcing appropriate trigger voltage and current, you can apply idea 1 (U23 is an open-drain level shifter)

    Unfortunately, I am not aware of a three position switch. LightCrafter E2E community might be able to help you.

    Regards,

    Divya

    www.ti.com/mems

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use