• Not Answered

Image on SD Card and image transmission


Actually I have two questions.


Is there any opportunity to save a set of images on the external micro-SD card and load them by a command?


While loading a BMP file the command looks like “02 01 05 01 e1 ff ….”.
In my opinion after “ff” the BMP values should be transmitted in case of black and white “00” or “FF” but there are still other values present. Did they represent the header information of the BMP?


Regards Andi

4 Replies