Hi!
I am trying to get a firewire camera to capture frames at the same frecuency that the lightcrafter is projecting images. What do I need to do?
According to the user's guide, I need to enable the output trigger from the GUI and then use pins number 3 (output) and 4(gnd) as my sync signal. However, as it is reported in a previous post (http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/850/t/185560.aspx) this does not seem correct. I have used an osciloscope and I have tested output pins 3 and 4 and I do not get any signal. Testing with a polymeter shows that they are both set to 0VDC.
Also, I can asses that I get these voltages, which do not make much of a sense according to the guide:
- pin1 - pin4 = 0 V (shouldn't it be 3.3V??)
- pin2 - pin4 = 3.3 V ( I am not using input sync, so I do not really know if this makes sense)
- pin1 - pin2 = 0 V
Thanks in advance,
Diego