To whom it may concern,
We are using the Lightcrafter with a Laser, therefore we removed the lightengine which worked quite nice for a few days. But after uploading an image with Matlab (always worked till this point), the image suddenly began to flicker. We tried rebooting, but it got stuck at the last bootscreen. After some more booting attempts the image now is always the same, it looks like the mirrors are randomly set to on- or off-state.
We tried to reinstall the firmware, the GUI connects but prompts "Command FAILED". The Firmware version are shown as:
DM365: 5.0
FPGA: XXX.XXX
MSP430: XXX.XXX
Updating the FPGA seems to work, since it says "Command SUCCESS", but its doesn't change anything. Updating the MSP430 doesn't work, its says "Command FAILED".
The LEDs seem to be ok. The one next to the DM365 blinks green/red, the other one on the top board is green, as is the one on the lower board.
The LightCrafter used ~0.2 A before, since the flickering it uses ~0.6A at 5V. The Voltage at the test points on the lower board are all as they are supposed to be.
We also tried the UART log and followed the instructions like this http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/850/p/176873/701728.aspx , but didn't get any information in tera term.
The last thing we tried was the I2C Software Reset, but just as our other attempts this had no effect. Here we are not completely sure we sent the command correctly, since it was the first I2C command we used, before we only used TCP/IP with USB.
I would appreciate your assistance since we have a deadline approaching shortly for which the DLP needs to function.
Thank you,
Dr. Benjamin Deissler
University of Ulm, Institute for Quantum Matter