Hi All,
I'm currently updating Firmware DM365 for LightCrafter DLP 0.3WVGA. I tried using the methods both booting from micro-SD card and from NAND flash. For the micro-SD card setup steps, I went through successfully-- formatted my micro-SD and got image copied just as images shown on the manual. However, after I inserted my micro-SD card to unpowered DLP LightCrafter, set DIP switch to the side of SD card, and power up DLP Light, the image got stuck at the top view of DLP (~90% progress) and the light near DM365 never turn green. Some people reported this problem and said that it could be solved by restarting the DLP through the button instead of unplugging.
http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/850/p/176873/1019042.aspx#1019042
However, that didn't work for me.
If anyone knows how to solve this problem, I'd greatly appreciate it.
Thanks in advance!
Guiping