Hi,
I used to program with my lightcrafter 3000 and control it to project static images, but recently I can't connect to the projector any more. In fact, the device can boot and show the RGB stripes normally and can be recognized by the computer when it's connected via USB. However, It can no longer be programmed with it, nor can it be connected using the GUI provided.
The weird thing is that no change has been made to any of the software which used to work properly. I did travel with this projector, but I don't think it's broken, but I do suspect there to be a hardware problem.
I also tried debugging with the sample code provided, and found that the method "send(sock, buffer + sent, length - sent, 0)" called in "int TCP_Send(int sock, unsigned char *buffer, int length)" in "tcp_client.c" returns -1.
Has anyone encountered the same problem before? Thanks in advance!
Best,
Xinyi