Hello,
I have another question. I tried to use the internal hardware pattern generator and experienced some problems with the sequence setup. Table 2-114 shows the sequence number (17) and the possible start and sub vectors settings. With these settings I did not get the correct pattern output. I got it working using the start vector 0x4B (from table 2-115). The subvecor does not seem to have an influence, but only the green led is working. I made the hardware changes to the driver board you suggested here: http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/850/p/362118/1273650.aspx#1273650
I set registers 0x4B and 0x4C to enable all three leds.
Is there a way to solve this? And what are the correct start vector and sub vector settings for the "Monochrome 1-bit internal pattern sequence with inversion" and "Monochrome 1-bit internal inverted pattern sequence" sequences?