Dear all,
I try to connect the PC with DLP Lightcrafter3000 using DLP LightCrafter GUI control software 5.0. But it fails. The GUI shows the message of “connection error =5”.
What I do are basically follow the instruction of “DLP® LightCrafter Evaluation Module (EVM) User's Guide”.
- Connect the DLP LightCrafter to the PC using a mini-USB cable.
- Turn on DLP LightCrafter using the on-off switch. A new network using the RNDIS driver should initialize.
But in this step, the Operate System can not automatically install the RNDIS driver. So, I have to download the driver of RNDIS/Ethernet Gadget and install the driver by myself. The following picture shows the installed driver ( in the list of network adapter).
3. Open the DLP LightCrafter GUI. Here the connection error occurs when I click the connection buttion in the GUI.
So, I think there must be something wrong with the driver. Why the installed driver is named as Android USB Ethernet/RNDIS Gadget #2? Is the connection error related to it?
In addition, my operate system is Window XP3, but it does not include the RNDIS driver, I think. So I have to install the driver manually.
So, could you give me some advices on fixing the problem?
Best wishes,