Hi,
Apologies for opening yet another topic, however this question is unrelated to the other one.
Uploading and displaying a sequence of 3 different 8-bit patterns works fine, but not at the proclaimed maximum refresh rate of 120 Hz. The max it seems to be able to achieve is 116.7 Hz, corresponding to a trigger period of 8568 µs. This is measured with a simple photodiode and oscilloscope and is consistent with the fact that whenever I try to set the trigger period to 8333 µs (corresponding to 120 Hz), and I run the sequence and "get" the lightcrafter stats again, the trigger period has suddenly gone back to 8568 µs. No matter what I try, it will not run at lower than 8568 µs...
I am on the newest Firmware upgrades for all subparts of the lightcrafter.
Any ideas?
Sam