Hi all,
I was developing some additional functions of LightCrafter on ubuntu based on "DLP LightCrafter Control Software -5.00". When I clicked the "Static Image/Test Pattern" tab then tested the "Static Image upload", the picture from "CustSeqInput "and "PatSeqImages" are projected properly, but the picture from "StaticImages" can not work. The Status bar just showed "Command Processing" and few seconds later, the whole GUI closed automatically. I even tested it out without doing any changes to the code after I downloaded the software bundles for linux, the issue still remains.
Thanks in advance.
Martin