Hi - I am having some trouble connecting to the device from my computer.
1- The device has turned on successfully I believe. It displays blue/green/red gradient and the PCB shows a green/red blinking light.
2- I am able to ping the device on 192.168.1.99:
C:\Windows\System32>ping 192.168.1.99
Pinging 192.168.1.99 with 32 bytes of data:
Reply from 192.168.1.99: bytes=32 time<1ms TTL=128
Reply from 192.168.1.99: bytes=32 time<1ms TTL=128
3- I am using Windows 8.1
4- I followed the instructions given in the user's guide and made it use the "Remote NDIS Compatible Device" drivers by Microsoft.
5- I also set the IPv4 properties to the above IP, the 255.255.255.0 subnet and 192.168.1.100 default gateway.
The GUI is unable to connect. I specified the correct address in the connections tab.
I either get nothing from it, or sometimes I get connection error 5. Hitting any of the get buttons gives me "No connection".
Any ideas about what to do next?
Thank you!