Dear friends:
Could anyone help me?
I want to use a Microcontroller STC89C52RC to generate the trigger signal. But the voltage of the pin of STC89C52 is 5V(TTL). However the LightCrafter's Instructions states that the voltage of the PIN2 of J7 should be 3.3V.
1、Could I connect the PIN of STC89C52RC directly to the PIN of J7 ?
2、If I can not connect the PIN of STC89C52RC directly to the PIN of J7,what should I do. Should I modify the Circuit board ? If I should modify the Circuit board,how to modify it. There is the board Board Schematic below.
3、where is the R282 on the board?