Hi Everyone,
First i want to say sorry if this is not the proper forum to ask my question because i was confused where to ask this kind of question.
Now my question is I want to design a projector which having the following specifications.
- Size of the projector should be as small as possible like EVM module of TI.
- DMD size at least 0.45'' (1280x800 )
- Light intensity around 500-700 lumens.
- Binary pattern projection speed 1200.
I have already bought LCR 4500 and Light crater EVM module. But problems with those projectors is there size are too big and those are not modular and alight intensity is quite low.
Is it possible to make a projector modular based ?Is there any other option we can built our projector.
The only problem with the commercial projectors is that there are so many functions which we don't need and 2ndly they can not project faster like LCR 4500.
Can anyone guide about this.