I have just received my DLP LightCrafter Evaluation Module EVM, but unfortunately it does not display anything, neither boot splash screen nor test patterns.
So far I tried the following.
1) Following the "Quick Start" guide contained in the EVM box. The Module seems to boot up correctly (D1 blinks red and green, D5 switch is green, the other one in the driver bottom board green). However, it has never displayed either the Splash Screen indicating that the system is booting, nor the test pattern that should appear when the boot is complete.
2) I connected the EVM to the PC with the mini-USB cable without problem. However, I can't visualize any of the test patterns. After I set any of the test patterns (both Internal Test Pattern and Stored Pattern Sequence) I always get a "Command SUCCESS" message, however nothing is displayed on the screen.
What do you suggest?
Thank you in advance.