Hi,
I want to use lightcrafter EVM to project simple colored graphical shapes like a green spot or red triangle (generated via Opengl) with specific intensity.
So for me what matters is being able to generate wide range of intensity values (256 steps for 8-bit ) at 60Hz . Also it is important that the output of lightcrafter at certain intensity level is stable.
I tried to do gmma correction to linearize the output of each LED over it's intensity range (using photodiode PDA-750 TetraHerz Technology ). But I found that all LEDs have certain fluctuation in their output around the mid range (0.3-0.8). something like this
for Red
for Green
and for UV
I obsereved same fluctuation both at 864x480 and 608x648 resolutions.
My question is what is the source of this fluctuation, is it from mirror control algorithm or is it from fpga.
If it from fpga, is there a way to modify it so it can generate stable intensity for each LED.
Thanks a lot in advance.
Best.