Hi,
We received a Lightcrafter EVM a couple weeks ago and connected to it via USB, and were able to control patterns using the GUI. We removed the light engine per the instructional video (Divya) and proceeded to test patterns using a HeNe light source (<1mW/cm^2). Unfortunately, we saw no pattern change and attempts to use pattern sequences failed to change the image reflected from the DMD. Commands sent via GUI returned command successful, so we reassembled the lightcrafter. Now on boot-up there is no splash screen, only a random, fixed binary image. We can change the current to the LEDs and when we switch modes from Static-->Test the projected image flashes. When switching to Pattern Sequence mode, the LEDs shut off until we load a pattern sequence and tell it to begin. We can control the duration, color, and trigger rate of the LEDs and uploading binary images returns "Command Success." However, no matter what image we use in Pattern Sequence, the same fixed random binary image is projected as there was at start-up.
Firmware Version
DM365: 5.0
FPGA: 2.6.43
MSP: 3.0
Is it possible that the DMD is damaged?
Any help is appreciated,
David