Are there CAD models available of the EVM module? The only annotated drawing I can find is the LightCrafter Base Plate Mechanical Drawing doc but that only has a small fraction of the overall dimensions I need. Specifically I need to align my models with the origin point of the lightcrafter's throw cone, which is somewhere inside the housing and not labelled. With that info, I can design in my mounting points for the base plate.