My LC3000 EVM is failing to boot no matter what I do.
I've seen several topics on the issue - but none have helped to solve my issue.
I am using the following FW versions: DLPC 1.0, EDID 1.0, FPGA 2.6.232, MSP430 3.0, DM365 5.0
Symptoms:
- DLP cycles through splash screens but never passes the 4th (last) screen - splash screens are all displayed correctly.
- No USB enumeration occurs (RNDIS device).
- LED states: D1=solid RED, D4=very faint GREEN (almost OFF), D5=solid GREEN, D3=off, D2=solid GREEN
Attempted:
- Booting from a SD card with both the NAND and SD card images - D1 LED stays RED.
- As no USB enumeration occurs - it is not possible to reflash the firmware.
Not sure what else I can try from here - perhaps I should try and read the MSP430 debug UART output?
Anyone have any other ideas?
Thanks.