Which are internal patterns and which are external?
I need to project binary frames as fast as possible, and then the difference between the internal frame rate (4000 Hz) and external (1440 Hz? (60Hz * 24)) is large.
Is the internal mode only when all of your frames are preloaded into the builtin RAM? If no,how else can I play frames in internal mode? If yes, does that mean even at lowest resolution I can only play few seconds of video at 4000 Hz? (4000 * 1 * 320 * 240 bits for each second)?
Any way some of the old frames can be removed from the RAM and new ones loaded while the animation is playing to not be limited to few seconds, yet still not drop to 1440 Hz (external mode)?
And can the RAM be upgraded by the user?