Hello,
I'm using the DLP LightCrafter as an intensity modulator. I have replaced the light engine with a collimated 532nm laser. However, I just couldn't display the desired 1-bit patterns / pattern sequences via the GUI. That is, whether I selected the Static, Test pattern, or Pattern sequence mode, the reflected laser didn't change at all, even though a COMMAND SUCCESS always appeared. The following is the tests I have done so far.
1. The splash screen was shown correctly. The intensity of the reflected laser changed from the typical grating to a blazed one. As far as I know, the default image is vertical bars after power-on. This was consistent with what I saw.
2. I tried to see the pattern change on the DMD by eye. The splash screen was correct again. However, no changes have been observed in patterns / pattern sequences. Even when all-white / all-black images were uploaded. BTW, my trigger period was 100,100 us with the AUTO mode.
3. To test whether I have broken the board when removing the light engine, I reconnected it and everything was correct as usual. Also, I observed that the LED shining on the system board was correct. Which is, two red and then one-red-one-green.
Now, I'm afraid this might be some problem with the GUI. FYI - my firmware version is DM365 5.0, FPGA 2.6.43, and MSP430 3.0. Can anyone help me with that? Thank you.