Hi, everyone.
I have big trouble using LCr EVM. I cannot connect the DLP LIGHTCRAFTER with my laptop.
The device can boot up and show the RGB stripes normally and can be recognized by the computer when it's connected via mini-USB.
However, It cannot be connected with the GUI provided. I checked the RNDIS network which is normal.
I've tried Win7 OS(32bit)_laptop and Win7 64bit another laptop. It shows "connection error = 5" or "connection error = 7"
I'm using the GUI, version is 'DLP LightCrafter FW & SW v5.0'. I've tried reinstalling RNDIS driver and rebooting LCr.
Please solve this problem.
Thank you! have a good day everyone :D