I was using DPL Lightcrafters evaluation module. In order to get a higher light intensity, I input a very high current value. The original value was 274 for all three LEDs, and I tried to input 400. Since I didn't see a higher light intensity, then I tried 500 and 600. I didn't feel any heat on the board, but now none of RGB light can be lit on. I have checked RGB LEDs using external a power source, it seems that the LEDs are OK, still working. What caused this problem? Is there any quick way to fix it? Thank you.