Hi all,
I have problems in connecting my DLP Lightcrafter via USB to my PC on a Linux system. I'm able to power on and boot it and I see RGB Color ramp pattern on the screen, but then when I connect it to the PC, it does not connect neither if I use the GUI nor if I run the lcr_app from the command line.
I read that there were problems related to the compatibility with USB 2.0, but only Windows was mentioned.
Does the same problems exist also on Linux and, if so, should I update the firmware?
Thank you in advance,
Valentina